Technical FAQs

Ask a Question

What is the short circuit rating of 9070 Type T control transformer with field installed 9070FB fuse blocks or 9070 Type TF (factory installed fuse block) control transformer?

These fuse blocks have rejection clips which require a Class CC rejection style fuses. Such fuses have an AIR of 200,000 amps.


CTA-ID : 2023241
Was this helpful?
What can we do to improve the information ?