Technical FAQs

Ask a Question

Are there optional aluminum compression lugs available for JD, JG, JJ, JL circuit breakers?

Yes, there are 2 different lugs available. Catalog number YA150JD is a set of 3 lugs with a wire range of 1 -#1/0 to #3/0 AWG AL or CU . Catalog number YA250J35 is a set of 3 lugs with a wire range of #3/0 to 350 kcmil Al or CU.


CTA-ID : 2023089
Was this helpful?
What can we do to improve the information ?