Technical FAQs

Ask a Question

What is the catalog number for copper mechanical lugs for JD, JG, JJ, JL circuit breakers?

Catalog number is CU250JD which is a set of 3 lugs with a wire range of 1 -#1/0 AWG to 300 kcmil CU .


CTA-ID : 2023087
Was this helpful?
What can we do to improve the information ?