Technical FAQs

Ask a Question

What is the catalog number for mechanical copper lugs for HD, HG, HJ, HL circuit breakers?

Catalog number is CU150HD which is a set of 3 lugs with a wire range of 1 -#14 to 2/0 AWG CU .


CTA-ID : 2023086
Was this helpful?
What can we do to improve the information ?