Technical FAQs

Ask a Question

What is the replacement for the two way pressure release valve for a 9013 FHGX pressure switch?

The replacement is cat. no. 9049 A56. Note that this is a replacement only, it cannot be added to a device which was not originally furnished with the two way pressure release valve (FORM X) from the factory.


CTA-ID : 2022949
Was this helpful?
What can we do to improve the information ?