Technical FAQs

Ask a Question

Do the EZM Metering branch devices come with any type of meter socket closing plate or cover?

Issue:
Current product design

Product Line:
EZM Metering

Evironment:
Product Features

Issue:
Product design

Resolution:
ALL the EZM Metering branch devices comes standard with meter socket covers for each meter position, BUT they DO NOT come with any type of meter socket closing plate, which is used to "Blank OFF' the meter position if there is No Watt-Hour meter in place. The closing plates MUST be obtained separately depending on the catalog number of the EZM branch device. SEE THE CURRENT DIGEST FOR PART NUMBERS.



CTA-ID : 2022946
Was this helpful?
What can we do to improve the information ?