Technical FAQs

Ask a Question

What is the D2 mean on the XMLA070D2S11 pressure switch?

D2 means the fluid controlled can be hydraulic oils up to 160 degrees C.


CTA-ID : 2022277
Was this helpful?
What can we do to improve the information ?