Technical FAQs

Ask a Question

Customer asks if the QO220EPD can be used at 240 Vac?

The QO220EPD is rated for use on a 120/240 Vac system whose phase to ground voltage does not exceed 120 Vac. The phase to phase voltage can be 240 V, but voltage to ground can not exceed 120 Vac.


CTA-ID : 2005543
Was this helpful?
What can we do to improve the information ?