Technical FAQs

Ask a Question

Can a QO circuit breaker still trip if a handle lock or clamp is installed in such a way that the breaker is locked in the on position?

Yes. All UL 489 listed circuit breakers are trip free.

CTA-ID : 2022459
Was this helpful?
What can we do to improve the information ?