Technical FAQs

Ask a Question

What replaces the mushroom pushbutton XY2CH13350 cable pull switch?

There is no direct replacement.
If the application permits look at possibly using the following:
Standard Push button XY2CH13150
Booted Push button XY2CH13250

CTA-ID : 2022760
Was this helpful?
What can we do to improve the information ?