Technical FAQs

Ask a Question

What is catalog number SL100?

It is a 100 amp rated, branch mounted sub-feed lug kit for use in I-Line panelboards. It will accept one # 14 to 1/0 copper cable or one # 12 to 1/0 aluminum cable.


CTA-ID : 2022749
Was this helpful?
What can we do to improve the information ?