Technical FAQs

Ask a Question

How is the ATV31 set up to operate by remote keypad?

With the VW3A31101 remote keypad kit installed, go to menu CtL and set parameter LCC to YES.
NOTE:  LCC can only be accessed if the drive controller is equipped with a remote keypad display, and if LAC = L1 or L2.
This function enables control of the drive with the STOP/RESET, RUN, and FWD/REV buttons on the remote keypad display.
The speed reference is given by parameter LFr in the SEt- menu.
Only the freewheel stop, fast stop, and DC injection stop commands remain active on the terminal block.
If the remote keypad display is not connected, the drive controller will lock on an SLF fault.

Reviewed 7/2011


CTA-ID : 2021698
Was this helpful?
What can we do to improve the information ?