Technical FAQs

Ask a Question

Is it possible to have the Altivar 31 run in keypad command but stop by means of a logic input on the terminal?

Yes. When the drive is in keypad command, the fast stop(FSt) and freewheel stop(nSt) inputs still function.  Go to menu FUn and submenu StC.  Set parameter FSt or nSt to the desired logic input. The stop will take place if there is not 24 VDC on the associated logic input.  When the 24Vdc is restored to the terminal, a new run command may be required.  See adjustable Speed Drive Controllers Programming Manual VVDED303042US for details.

Reviewed 7/2011


CTA-ID : 2021696
Was this helpful?
What can we do to improve the information ?