Technical FAQs

Ask a Question

Is the SDT2100 branch circuit breaker still available?

The SDT2100 is no longer available. The only alternative is to purchase a complete 100 ampere Main Breaker Interior, SDTN20M100. The SDT2100 provided with this interior can be used as a branch breaker on 150 and 200 ampere mains Trilliant panels.

CTA-ID : 2022217
Was this helpful?
What can we do to improve the information ?