Technical FAQs

Ask a Question

What is the coils resistance for a 8501KP, KF and KU relays?

+/- 10% @ 20 Degree C for DC coils ---
28 ohms at 6 volts, 110 ohms at 12 volts, 430 ohms at 24 volts, 1750 ohms at 48 volts, 9200 ohms at 110 volts, 1000 ohms at 125 volts,
-/+15% @ 20 degree C for AC coils----
4.3 ohms at 6 volts, 18.5 ohms at 12 volts, 75 ohms at 24volts, 305 ohms at 48 volts, 1910 ohms at 120 volts, 7760 ohms at 240 volts


CTA-ID : 2022736
Was this helpful?
What can we do to improve the information ?