Technical FAQs

Ask a Question

Are the H364N, H364NA, H364NAWK, H364NDS and H364NRB safety switches Suitable for use as Service Equipment?

Issue:
Application

Product Line:
HD Safety Switch

Cause:
Application

Resolution:
Yes, these switches are marked: "Suitable for use as service equipment". For service equipment use the neutral should be bonded to the enclosure with the green neutral bonding screw provided with the switch.


CTA-ID : 2022735
Was this helpful?
What can we do to improve the information ?