Technical FAQs

Ask a Question

Can the QO13040L200WG wide-gutter load center be converted to a main breaker load center?

Yes, it is convertabe to main breaker when QOM2 frame size breaker is installed (200A maximum). Note that when converted to main breaker, the cover must be QOC30UFWG, since the NQC30FWG does not have a knockout for the main breaker.


CTA-ID : 2022742
Was this helpful?
What can we do to improve the information ?