Technical FAQs

Ask a Question

Are alternate lugs available for the MP22125, MPR22125 or MPH22125 Meter-Pak devices?

Issue:
Product accessories

Product Line:
MP Meter Pak

Environment:
Main Lugs

Cause:
Wire sizes

Resoution:
No. the MP22125, MPR22125 or MPH22125 will not accept alternate lugs. So the lug kits MMLK250, MMLK500 or MMLK600 lug kits CANNOT be used on these devices.


CTA-ID : 2022430
Was this helpful?
What can we do to improve the information ?