Technical FAQs

Ask a Question

I have an EZM1600FS main box and there is a 1/2`` gap between the buses. Is this normal?

This is a main fusible device. The gaps are there for the installation of fuses. The disconnect in the box is a molded case switch, not a circuit breaker.


CTA-ID : 2022422
Was this helpful?
What can we do to improve the information ?