Technical FAQs

Ask a Question

What is the software for downloading test information to a computer from the Micrologic Full Function Test Kit?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Order CD catalog number FFTKRPT-V1-0 on Q2C. A customer-supplied serial (RS-232) cable is also required to connect from the FFTK to the computer.


CTA-ID : 2022166
Was this helpful?
What can we do to improve the information ?