Technical FAQs

Ask a Question

What box does he use with the GS504NI?

Issue:
Selection

Product Line:
Medical Panels

Environment:
NFPA99, NEC517.160

Cause:
This product ships without box, which is ordered separately.

Resolution:
The GS504NI is obsolete.  Please see FAQ number FA110430 for replacement information.  GS504NI mounted in any metal 4 gang box will do that is 3.5 inches deep maximum.  The GS504 has only 4 ground jacks.


CTA-ID : 2022581
Was this helpful?
What can we do to improve the information ?