Technical FAQs

Ask a Question

What is the AIR rating of an LAL36350 breaker at 240V?

The IC rating of that breaker is 42 kA @ 240 Vac


CTA-ID : 2022408
Was this helpful?
What can we do to improve the information ?