Technical FAQs

Ask a Question

What are the interrupting characteristics of GDL breaker? <br />NOTE: this is different from the GJL which has a 65 kA rating @ 480 Vac

25KA at 240Vac.
18KA at 480Vac.


CTA-ID : 2022161
Was this helpful?
What can we do to improve the information ?