Technical FAQs

Ask a Question

Are the EZML metering units rated for cell towers, CEHHA or Con ED certification?

Yes. Those units are certified and rated for use in those jurisdictions.


CTA-ID : 2022911
Was this helpful?
What can we do to improve the information ?