Technical FAQs

Ask a Question

What is the require torque for the lugs for the QOM2200VH main breaker in the QO and Homeline load centers?

Torque is 250 lb.-in. or 28 N-m.


CTA-ID : 2022708
Was this helpful?
What can we do to improve the information ?