Technical FAQs

Ask a Question

Is there a QOB 3 pole 60 amps which has a 415Y/240 voltage rating?

The QOBXD363 is rated for 63 amps 240 volts maximum and is for export use in a 415Y/240 NQODX panelboard.

CTA-ID : 2022574
Was this helpful?
What can we do to improve the information ?