Technical FAQs

Ask a Question

What does the C1H suffix indicate on a QOU115C1H.

This is a special made for Crouse Hinds. Off end of breaker back by the lugs there is material removed at a 41 degree angle on both sides of breaker. To fit into their equipment.

CTA-ID : 2022565
Was this helpful?
What can we do to improve the information ?