Technical FAQs

Ask a Question

How many and what size conductor(s) will the Class 9422 Type TF* variable depth flange mounted disconnect accommodate?<br /><br />* = 1, 2 or 3

The lugs are aluminum single barrel design which will accept (1) # 6 AWG to 300 MCM aluminum or copper conductor per phase.

CTA-ID : 2022365
Was this helpful?
What can we do to improve the information ?