Technical FAQs

Ask a Question

Is the 2601 ball and shaft handle made of metal?

Yes. This optional handle is all metal except for the round plastic knob on the end. It consists of three parts: plastic knob, steel shaft, die cast zinc base hub.

CTA-ID : 2022364
Was this helpful?
What can we do to improve the information ?