Technical FAQs

Ask a Question

Does the Q22200NS, Q23225NS, Q23225NF and Q23225NRB included a solid neutral assembly?

Issue:
Product Design Features

Product Line:
Q Frame Circuit Breaker Enclosures

Environment:
Solid neutral 

Cause:
Application

Resolution
Yes, the 'N' in the catalog number shows that the enclosures come with a Solid Neutral assembly included. The neutral is insulated from the enclosure but a bonding screw is provided if needed for Service Equipment applications. 


CTA-ID : 2022351
Was this helpful?
What can we do to improve the information ?