Technical FAQs

Ask a Question

Can the ATV31...A model be setup to use the integral speed pot dial for reference adjustment, but use the LI logic input for a run forward command?

Yes.  In the IO menu, set parameter tCC to 2C.  This assigns LI1 as run forward command.  In the CtL menu, set parameter Fr1 to AIP.

Reviewed 7/2011


CTA-ID : 2021451
Was this helpful?
What can we do to improve the information ?