Technical FAQs

Ask a Question

How do you enter a hot sequence meter section on the secondary of a medium voltage transformer in the Product Selector / Configurator?

As of 3/7/05 there is not a standard connection from a hot sequence meter section on the secondary of a medium voltage transformer? To enter this in the Product Selector / Configurator TAG IN the transformer connection and enter the meter section as having incoming cables.


CTA-ID : 2022538
Was this helpful?
What can we do to improve the information ?