Technical FAQs

Ask a Question

What is the part number for the busway joint cover on AP502G10?

Tie channel plates are catalog number 45202-026-01. Two required per joint. The screw bag (to attach the tie channels to the busway) is 45132-001-55. One screw bag is required for each busway joint.

CTA-ID : 2022326
Was this helpful?
What can we do to improve the information ?