Technical FAQs

Ask a Question

Does Square D manufacture a 400A CSED with a single 400A main breaker?

Issue:  
Can you use a CSED to feed 400 A from a single disconnect?

Product Line:  
Residential electrical distribution

Environment:  
Combination Service Entrance Devices (CSEDs)

Resolution:  
Yes, we have the following CSEDs which include a 400 A main breaker disconnect to feed out directly.  The CUM400CB is ring type and the QUM400CL and QUM400CK are ringless type.  They will all include an LJL36400U31X main breaker.  

NOTE:  These may also be modified to accept two 200 A Q-frame breakers to feed downstream load centers.  The Q-frame breakers must be purchased separately and you MUST also purchase the installation kit BMK2Q400 to make this conversion.  
Was this helpful?
What can we do to improve the information ?