Technical FAQs

Ask a Question

What enclosures are available for an LEL circuit breaker?

Only one enclosure, LX600AWK, is available for the LEL frame circuit breaker. Use this enclosure for NEMA 1, NEMA 3R, NEMA 5 or NEMA 12 applications. This enclosure is also applicable to the LXL, LXIL, LCL and LIL frame circuit breakers through 600 ampere. NOTE: The LEL breaker, when using a 600 ampere sensor, is only rated for a 80% application.


CTA-ID : 2022527
Was this helpful?
What can we do to improve the information ?