Technical FAQs

Ask a Question

How do you tell if the battery in an ALAM is OK?

Issue:
Battery Check

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Cause:
Checking battery status.

Resolution:
With the ALAM installed, a battery OK symbol should show when the button is pressed.


CTA-ID : 2035477
Was this helpful?
What can we do to improve the information ?