Technical FAQs

Ask a Question

What is the function of a 1212 suffix on a KAL362001212? What is a 1A/1B auxiliary contact?

The auxiliary contact is a (one normally open/one normally closed) contact that mirrors the on or off status of the breaker. It is usually connected to a low voltage control or monitoring circuit.


CTA-ID : 2035435
Was this helpful?
What can we do to improve the information ?