Technical FAQs

Ask a Question

Does the ATV58 Autotune parameters change the motor parameters when set the tUn parameter to yes and it changes from Done to No?

Yes. The motor parameters revert to Factory default.


CTA-ID : 2022454
Was this helpful?
What can we do to improve the information ?