Technical FAQs

Ask a Question

What are the ratings of the contacts on suffix 1212 of a FAL breaker?

They are 10A at 120V - 240VAC, 1/4hp at 120V - 240VAC, 0.5A at 125 Vdc


CTA-ID : 2022513
Was this helpful?
What can we do to improve the information ?