Technical FAQs

Ask a Question

What is required to convert from class H to class J fuses on a 9422TG2 disconnect switch?

The lower fuse clips must be moved up to accommodate the Class J fuse. The fuse clips can be relocated to accommodate 250 and 600 volt class H fuses and 600 volt class J fuses.


CTA-ID : 2022497
Was this helpful?
What can we do to improve the information ?