Technical FAQs

Ask a Question

Is a replacement NEMA 7 & 9 or NEMA 7, 9 & 3R enclosure available for the Class 2510 Type M available?

Issue: Is a replacement NEMA 7 & 9 or NEMA 7, 9 & 3R enclosure available for the Class 2510 Type M@# available? @ = B or C, # = R or T

Product Line: 2510 type M and T integral horsepower starters

Environment: Products sold and used in the United States

Cause: Replacement NEMA 7 & 9 or 3R enclosure for 2510 type M manual starters

Resolution: No, we do not offer replacement enclosures for hazardous location devices.




CTA-ID : 2016391
Was this helpful?
What can we do to improve the information ?