Technical FAQs

Ask a Question

Is there an option for factory installed four position High - Low - Auto - Off selector switch for the Class 8810 two speed starters?

Yes, use factory modification Form C25 when ordering.


CTA-ID : 2022668
Was this helpful?
What can we do to improve the information ?