Technical FAQs

Ask a Question

Are the Class 8810 Type S two speed starters available in a NEMA 3R enclosure?

No, the two speed starters are only available in NEMA 1, 4, 4X, 7 & 9 or 12.


CTA-ID : 2022287
Was this helpful?
What can we do to improve the information ?