Technical FAQs

Ask a Question

Can 8430MPSV24 be used to monitor a 208V system?

Since the undervoltage feature is adjustable down to 180V, it can be set at desired protection level within the 180V to 208V range. So yes, it can be used.

CTA-ID : 2022789
Was this helpful?
What can we do to improve the information ?