Technical FAQs

Ask a Question

What are the dimensions of a MH674?

Issue:
What are the dimensions of a MH674?

Product Line:
NQOD Enclosure and Accessories

Environment:
Products sold in North America

Cause:
Need dimension of the MH674

Resolution:
74`` high, 20`` wide, and 6.75`` deep.

The MH674 and blank end wall replacement (80110-319-01) are obsolete.


CTA-ID : 2022786
Was this helpful?
What can we do to improve the information ?