Technical FAQs

Ask a Question

Can a customer get an aluminum lug instead of the clamp-plate on QO low-amp breakers?

To get an aluminum lug on the HOM or QO 10-30 Amp breaker, order with a 5219 suffix. The price is higher.

CTA-ID : 2022669
Was this helpful?
What can we do to improve the information ?