Technical FAQs

Ask a Question

What is the electrical interlock for use with the HU365DS Series E4?

Issue:
product design features

Product Line:
Heavy Duty Safety Switches

Environment:
Accessories

Cause:
Application

Resolution:
THe HU365DS Series E4 can use the EIK40601 for 1-NO/1-NC contacts and the EIK40602 for 2-NO/2-NC contacts.


CTA-ID : 2022475
Was this helpful?
What can we do to improve the information ?