Technical FAQs

Ask a Question

What is a 9001 AS2?

Issue:
What is a 9001 AS2?

Product Line:
Harmony Push  Buttons

Environment:
All 30mm Push Buttons

Cause:
Kit compnents

Resolution:
This is a member of the Point of Purchase, or POP, system. These are devices packaged in plastic clam shells to display on a peg board at a distributor. The 9001 AS2 consists of a 9001 KS43BH13 and a 9001 KN260.


CTA-ID : 2022285
Was this helpful?
What can we do to improve the information ?