Technical FAQs

Ask a Question

What amperage is a ARP100?

The rating plug does not determine the amperage. It is used as a percentage multiplier to multiply with the breaker sensor and the long time pick up set point. The ARP100 is a 100% multiplier, so when it is installed, the breaker's sensor rating is the amperage multiplied by the long time pick up set point.


CTA-ID : 2022776
Was this helpful?
What can we do to improve the information ?