Technical FAQs

Ask a Question

A customer wants a manual for the trip unit on an automatic switch.

The DIN function is integral to the automatic switch and there is no separate manual for it.
The automatic switches have the same ``DIN`` (instantaneous override) function as the standard breaker, but they do not have the LSIG functions.

CTA-ID : 2022774
Was this helpful?
What can we do to improve the information ?